Hello, I use this chip CC2652P.During testing, I found that using the interrupt callback function provided by the SDK, the interrupt response was 70us, which was too long, so I used the IOCINT registration (void (* PFNHandler) function in the lib library to reprocess the call from the interrupt source.When an interrupt is triggered, I use the GPIO_clearMultiDio function to remove the interrupt flag bits.But after a long and quick rest.The interrupt cannot continue, I want to know if there is anything in the interrupt source that I have not done.At the same time, I changed the trigger function of the interrupt source, but the interrupt response time was still too long.I saw your company's description at interr_doc.h that a small delay was added before the interrupt source.I wonder if there is any other way to deal with this problem。
Thanks!