This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL18XXCOM82SDMMC: Failed to Load BTS script using HCI Tester tool.

Part Number: WL18XXCOM82SDMMC
Other Parts Discussed in Thread: WL1837,

Hi all,

We are planning to perform RE testing for the WL1837 module with the WL18XXCOM82SDMMC setup. We are facing some issue when trying to load the BTS script to the device using the HCI Tester tool. When we run the attached BTS script, we get the following error.

01:45:56.702 ERROR - File: "C:\Users\Desktop\BT_Testing\Bluetooth_testing\TIInit_11.8.32.bts", Line: 1
01:45:56.703 ERROR - Script parse Error
01:45:56.703 ERRORed Line (1): BTSB
01:45:56.704 Script: C:\Users\Desktop\BT_Testing\Bluetooth_testing\TIInit_11.8.32.bts  -- Aborted

The same script is working properly in the linux OS running on IMX6 processor. We would like to know the exact steps to run the BTS script using the HCT Tester tool in the WL18XXCOM82SDMMC.

When the WL18XXCOM82SDMMC device is connected in the windows host PC, there are 4 serial port enumerated. Kindly, let us know which serial port needs to be used for communicating with the BT interface.

TIInit_11.8.32.zip

Regards,

Sudar