The customer wants FCC certification, but has a question: 1. Does CC2571 have a communication channel? 2. Is the output frequency range 2400-2485mhz or 2495Mhz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The customer wants FCC certification, but has a question: 1. Does CC2571 have a communication channel? 2. Is the output frequency range 2400-2485mhz or 2495Mhz?
Hi,
Please refer to the product page (https://www.ti.com/product/CC2571) and the datasheet of this part (https://www.ti.com/lit/gpn/cc2571).
CC2571 Supports Eight ANT Channels.
As you will see, the device is able to transmit between 2400 and 2495 MHz, however, the ANT protocol only uses the frequencies between 2400 and 2485 MHz.
Best regards,
Hi,
Eight ANT Channels?How do we divide frequencies?
ANT channels are not decided by frequencies. Please refer to the documents I have pointed you to.

I hope this will help,
Best regards,
Hi,
As a reminder, FCC certification is done at the systems level - not at the device level. See here for details.
CC2571 is suitable for Systems Targeting Compliance with FCC CFR47 Part 15 • Consumer Health Devices(US).
Best regards,