Other Parts Discussed in Thread: TRF7970A
Hello
I use MSP-EXP430F5529LP example with DLP-7970ABP, as i run example of card emulation (type 4A,4B), it takes 5-10 seconds to read emulated card with my phone, how can i reduce that time ?
the problem also is, that if u wanna read, u cant just hold the phone and wait until it reads, u have to move around near antenna and looking at the led (which is blinking when externald field is detected) to catch right position
y