Hi,
I'm looking for the part specific header files "ioCC2510.h" and "ioCC2511.h". These are also used by swrc088c and swrc117, but where do I get them from?
Thanks,
Rene
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm looking for the part specific header files "ioCC2510.h" and "ioCC2511.h". These are also used by swrc088c and swrc117, but where do I get them from?
Thanks,
Rene
Hi Rene,
Look inside your IAR EW8051 install folder. For example, mine are located in C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\8051\inc
Regards,
Ryan
So I really have to register at IAR just to download software I'm clearly not going to use only to get the header files??? Do these files still contain the KEIL definitions, as the files for the CC111x already in use? BTW, where did I get these files from? IAR was never installed on my systems...
Attached are the files for your reference. For further CC251X project development you will need a compatible IDE. IAR offers trial versions for limited-time evaluations.
Regards,
Ryan
I'm using KEIL, this is hopefully compatible enough (at least, it has been compatible enough for the CC1111 for more than 10 years now). But however it is, using IAR is not(!) an option.
Thank you very much for the files!
Rene