Hi i have a few questions regarding frequency change on Microreader RI-STU-MRD2
In the document scbu049: 6.4.3.26 Execute C-Trimming (Command 0x43)
This command starts a C-trimming sequence to adjust the transponder resonance frequency to a given
target frequency. Because this procedure is device-dependent, the additional specification of the device is
necessary. The target frequency must be specified in Hertz. For example, a target frequency of 02 0C 38
equals 134.2 kHz.
This command does not work
What I wish to do is to change the transmitter frequency to 125kHz
Is the asked frequency out of range for the product perhaps im telling it to go for 125kHz