Part Number: WL1835MODCOM8B
Hello,
We are working on a product that uses wifi as well as Bluetooth both the feature on TI chip. We are seeing a very frequent connection and disconnected of wifi network from one AP to another only in a case when both the APs have same SSID but different BSSID. Wifi is flapping mostly every min or so. Our team need help to find out the root cause while we are trying different configurations at our end.
Here is the platform details:
Bluetooth firmware: TIInit_11.8.32.bts Version : TI_P2.147
Wifi firmware:
WL18xx MAC firmware version 8.9.0.0.86
WL18xx PHY firmware version 8.2.0.0.245
BlueZ stack 5.55
Linux 4.14.98+
APs are standard Cisco Meraki dual band 802.11n multi-ap enterprise setup with band and congestion steering. I have attached the wpa_supplicant config and our device specific config used to configure TI firmware. I have also attached a small snippet of kernel logs whenever these disconnection happens.
Let mw know if TI team needs more information.
Thank You!!
wpa_supplicant.rtf
Kernel Log.rtffiles.zip