Other Parts Discussed in Thread: RF430FRL152H
Hi,
Context : I'm trying to use your development kit RF430FRL152HEVM with Vbat =1.5V in order to run an I²C communication with an external sensor, to read the value and to save it in the ROM. Then, when the device is not being supplied by Vbat, I want to read the information of the sensor saved in the ROM via the NFC.
My sensor is working with signal that toogles from 0V to 1.5V, so I removed the level shifter on the developpement kit to access directly to the I²C pin's signals of the RF430FRL152H. I also needed to apply a voltage supply of 1.5V on RST/NMI in order to feed the integrated circuit. But when I do that, the voltage of 1.5V which is the high voltage reference of the I²C communication decreases over the time (SDA & SCL), then the high voltage reference is lowering from 1.2V to 900 mV, why not a stable 1.5V ?
I would like to know if you have any solutions to run the RF430FRL152H with a 1.5V voltage supply ?
Thanks in advance,
Gaëtan Andrieu.