This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2662R-Q1: No communication between nodes

Part Number: CC2662R-Q1


Hello,

Is it possible to establish a communication between two WBMS EVM nodes without supplying the 12V power? (battery monitor devices not powered)

I am trying to establish communication between a main node and a single wireless node - both are currently powered by the XDS110 Debug Probe with CCS in debug mode (no 12V supply is being provided)

The wmain and wdevice firmwares have been uploaded successfully to the MCUs as per the instructions from the wbms quick start guide in the SDK. However, when macStats expression is inspected, there is no data or communication between the two nodes.

Thanks for your help.

Toby Brown

Field Application Engineer Intern (UK)