Other Parts Discussed in Thread: MSP430F5529
Hi guys,
Has anyone successfully port the TRF7970ABP_RFID_Reader_Demo to run on the launch pad with the MSP430F5529 (https://www.ti.com/tool/MSP-EXP430F5529LP)
When I retarget this demo project in code composer to MSP430F5529, I start getting errors in mcu.c, spi.c and uart.c
I can remove uart.c as I don't need that functionality but not sure on spi ones as these are tightly coupled with the main trf7970.h / .c files.
In spi.c I get these errors
line 139
while (!(IFG2 & UCB0TXIFG));
line 295
P1SEL2 |= BIT5 + BIT6 + BIT7; // P1.5,1.6,1.7 UCBOCLK,UCB0SIMO,UCB0SOMI, option select
in mcu.c
get errors in MCU_initClock.
If I do rectify the errors will the IO pins still map eg will chip select map correctly on the launch pad to the DLP 7970-ABP?