Hi there,
I have customer who is evaluating the CC2530 which is to be used in their tablet-style menu system, where customer can use it to place order directly.
They also need to use it for positioning purposes as they are afraid that the customer might bring the device out of the restaurant.
The CC2530 uses the RSSI to determine this, however the accuracy drops beyond 10 meters.
They are also looking at NXP's JN5148 which uses the Time of flight (TOF) protocol when the distance is beyond 15meters. Customer is now more interested in the NXP part as they are able to use this TOF protocol to calculate the distance more accurately and this is important to them.
Does TI have anything to offer, which the accuracy of the distance calculation is maintained even beyond 10 meters?
The maximum distance they are looking at is about 15meters.
Below is a portion which is taken off the NXP JN5148 datasheet.
8.5 Location Awareness The JN5148 provides the ability for an application to obtain the Time Of Flight (TOF) between two network nodes. The TOF information is an alternative metric to that of the existing Energy Detect value (RSSI) that has been typically used for calculating the relative inter-nodal separation, for subsequent use in a location awareness system. For short ranges RSSI will typically give a better accuracy than TOF, however for distances above 5 to 10 meters TOF will offer significant improvements in accuracy compared to RSSI. In general, the RSSI error scales with distance, such that if the distance doubles then the error doubles. Please advise Thank you! Adam