Other Parts Discussed in Thread: UNIFLASH
I’m writing to bring your attention some technical issues that i have encountered while testing the CC2662RQ1-EVM-WBMS and the XDS110 Debug PROBE.
- Firstly I have been experiencing frequent connectivity issues with the XDS110 debug PROBE. I tried to plug in the XDS110 to my PC via USB and the AUX port breakout board connected to the AUX port, I expected to be able to measure 5V at the TGTSUPPLYOUT pins but I'm not seeing any voltage.
- Secondly, after many tries the voltage measured between TGTSUPPLYOUT and GND is only 0.6V even after keeping the configuration to “Probe supplied power”.
- In addition, now i can’t even detect the XDS110 probe Debug using the UNIFLASH and also i can’t find the CC2662RQ1-EVM-WBMS in the list of the Ressource Explorer or even in the UNIFLASH.
I contacted an IT technician on the platform, he told me that the CC2662RQ1-EVM-WBMS in question is an obsolete product.
Thank you for your attention to this matter.