Hi Team,
Product: Indoor Photolamp equipment
Packet definitions and basic concepts:
The customer's packet contains two bytes of sync word. Normally, the sender automatically inserts the sync word, and the receiver detects if the received sync word is the same as the agreed sync word. If yes, the CC2500 will automatically upload the data packet to the master MCU; if not, the cc2500 will not upload any information to the master MCU.
In the customer's product, the sync word is called ID. A total of 100 IDs have been defined.
Issue: Communication frequency point settings on both transmit and receive side. However, some IDs can also communicate with each other in cases where the ID settings are different.
For example, the receive side is set to ID0, regardless of the transmit side is set to ID0, ID1, ID3, Either ID7 or ID7, can communicate with the receiving end. Communication is best with the transmit side set to ID0; setting to ID1, ID3, ID7 has a small possibility to communicate.
The associated IDs are defined as follows: