This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS37157: Communication problems between TMS37157 and TMS37157

Part Number: TMS37157
Other Parts Discussed in Thread: RF430CL330H, TRF7970A

1. I have a need for short-distance communication, the maximum distance is about 1CM, the two devices are equivalent, using the same chip.
2. The chip needs to support low-power mode, because it is a small device and needs to support 3 years of work.
3. The requirement of communication rate is not high, only a simple exchange of ID information is needed.
4. TMS37157's existing scheme is to communicate with the card reader. Does this scheme support the communication between TMS37157 and TMS37157?  that is, the device is required to initiate communication actively.
5. I have also looked for other similar solutions, such as NFC (frequency is 13.56Mhz), such as RF430CL330H, but P2P peer-to-peer mode is not allowed.
6. Is there a solution that supports peer-to-peer or reader/writer modes that can be recommended to meet my requirements?