Hello Team,
I have the following use case. Can you please confirm if TRPGR30ATGB will work or you will suggest another part?
--------------------
A hole should be drilled into a concrete floor where the transponder can be inserted with a rubber mallet. The transponder should then be able to be read at a maximum distance of 20cm above the ground. There can be water
in the hole and above the transponder and it must still be readable. The transponder must be acid (cattle manure) resistant. Do you have something suitable?
I don't know if that's something suitable... the shape would fit:
www.mouser.de/.../595-TRPGR30ATGB
Maybe I can also drill the holes a little larger so that the transponder doesn't have to be pushed in with a hammer and then close them again.
--------------------
Thank you in advance.
Best Regards,
Usman Niazi
QEC45E9