Hi Team,
I have a machine here using the CC2500 module that can receive normally at first, but cannot receive after a while.
I switch the mode to transmit, and the module can work normally, but it just cannot receive, and the software reset and initialization does not work.
It must be Just power off and on again. After the RF receiver crashed,
I used a normal machine to compare it with a logic analyzer and found that the RF after the crash could receive data, but the data was wrong and the number of bytes did not match.

I have re-initialized the RF when switching modes, but it doesn't work. I can still only send but not receive. The CC2500 module must be powered off and on again.

This is the vedio.
Best Regards,
Galaxy