Tool/software:
Hello,
I am developing a wireless MIC and USB receiver system using the CC8531 in host-controlled mode (with USB receiver as the protocol master and MIC as the protocol slave).
I need to know about the automatic rejoining of a protocol slave once it goes out of network range.
Is this functionality already available in the "host-controlled operation" of the CC8531, or do we need to code the host controller to perform an NVM_DO_SCAN again to rejoin the network?
If the host controller has to implement this, should the scan be initiated from the USB receiver side or the MIC side?
Please provide some solutions along with reference documents if possible.