Other Parts Discussed in Thread: RI-STU-MRD2
Tool/software:
Hi all,
I am currently using the Protagd PRDG23WS Read/Write transponder with the MRD2EVM Reader with own custom C# code, sending bytes to the reader to perform read/write actions. I’m having troubles with sending the bytes to the reader to write the transponder.
Reading using ECM and LMP methods both work, but I am unable to write using either methods. Here are my bytes for the following functions. Data fields (8 bytes) and the BCC field are added dynamically so they're just set to 0 for the command format. These are written with reference to the RI-STU-MRD2 Reference Manual:
ECM Read (Pg42): { 0x01, 0x03, 0x80, 0x01, 0, 0 }


ECM Write (Protagd Manual Pg12) { 0x01, 0x0B, 0x80, 0x21, 0x15, 0, 0, 0, 0, 0, 0, 0, 0, 0 }

(For ECM Write (Pg43), I am not sure what is the 'Keyword' and 'Password' field. I have tried using the ECM Write command and using 0, 0 for the 'Keyword' and 'Password' field, and I have also tried reducing the length to 0x0B and omitting the 'Keyword' and 'Password fields', but both does not work.)
For ECM Write, I am getting a response code 01-02-05-00-07, giving me error code 0x05.
LMP Read (Pg24): { 0x01, 0x02, 0x08, 0xFF, 0 }

LMP Write (Pg25): { 0x01, 0x11, 0xE8, 0x06, 0xFF, 0x0F, 0x0C, 0xBB, 0xEB, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0x03, 0 }
(I am not too entirely sure what byte numbers 17 and 18 (Data field 14-15: Write Frame) is supposed to be, but according to old source code by my colleague, it was set to 0, 3. I've also tried to use the command without both fields, did not work either)

I've reached out to Protagd, and was told that the TI MRD2EVM reader is not compatible with the Protagd transponders, however, we do have another version of the custom software that is able to read and write to a Protagd transponder using the same TI reader. Only problem is that nobody is able to find the source code for that.
Would appreciate if anyone could advise on whether the bytes sent were wrong, or where should I look for the error. Thank you in advance!
Edit: attached both manuals for your reference