Other Parts Discussed in Thread: CC2590
Tool/software:
Hello,
I am reaching out because I’m considering using the CC8530 series for a commercial application.
As such, I cannot share my schematics publicly, but I can provide them privately if needed.
Since the evaluation kits are no longer available, I have designed two custom boards (one transmitter and one receiver) based on the CC8530 + CC2590.
I took an example project from PurePath Wireless Configuration (the CC85XXDK Preloaded Demo) and flashed these example programs onto my boards.
The program writes successfully, and I can see the LED briefly blink once per second (indicating the ALONE status).
However, I am unable to enter pairing mode.
I tried both pairing methods:
Proximity pairing: pressing the pairing button on the Slave while enabling Proximity Base Pairing on the Master.
When I press the pairing button on the Slave, the LED never blinks twice as it should according to the default status indications.
Protocol Master Pairing Signal: pressing the pairing button on both Master and Slave.
I can see the LED blink twice on the Master when the button is pressed, but this never happens on the Slave.
When I press the pairing button on the Slave, nothing happens.
I suspected the issue might be hardware-related, but when I flash the Master program onto my Slave board, the LED correctly blinks twice when I press the button.
As soon as I re-flash the Slave program, the double blink no longer occurs.
At this stage, I am unable to initiate any pairing.
I also tried using PurePath Wireless Commander, where I ran a production test using the default prod_test_pairing.ppwptc script.
I successfully pass the first two steps (Program Autonomous Application Master & Program Autonomous Application Slave), but the Pairing Autonomous Master/Slave step always fails with the following error:
WASP network formation failed (status: 8a05)
I have, of course, verified that my pairing filters are empty, and checked my I/O mappings, etc.
I have also checked crystal, which is fine (48Mhz at measurement).
Could you please advise what might be causing this issue?