This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2400: Connection between the pin 1 marking on the backside and AGND

Part Number: CC2400


Hi team,

On the backside of the CC2400, the pin 1 marking was connected to the center AGND of the component.

Was this connection defined in the specifications of the device? 

Also, has the connection between the pin 1 marking and AGND been part of the specifications since the initial release of the IC?

When the customer mounted the component on the board, there was a power through-hole near the pin 1 marking on the backside of the component.

The pin 1 marking came into contact with the power through-hole, resulting in a short circuit between power and GND.

As a result, an investigation was conducted and it was found that there is electrical continuity between the pin 1 marking and AGND.

Thank you in advance for your response. 

Best regards,
Masahiro Kobayashi