Other Parts Discussed in Thread: TPS1689
Hello team,
TPS1689 is not properly starting up if there is Rload of 15ohm.
(Customer has disabled TPS16851VMAR by populating R81 and R84.)
Setup Condition:
VIN: 43V
Load: 15ohm
dv/dt: 0.1V/ms
The startup waveform is below.
VOUT goes to 0V after 40ms.
What might be the problem here? Might it be thermal shutdown?
Can TPS1689 send fault status of thermal shutdown via PMBus?
Best Regards,
Kei Kuwahara