Hi,
I have custom board with CC1100E as a transmitter. SPI communication works fine. According to the manual and SmartRF setting PKT_FORMAT=3 will turn GDO0 into a TX input. Do I need to configure anything else before I may apply signal to the GDO0 pin and start transmission? Is GDO0 an input now? The manual mensions something about GDO0_Z_EN_N configuration settings for GDO2 to use GDO0 as input.
What kind of TX signal can I transmit? Can I directly control RF output by toggling GDO0 or it should be NRZ or something? As for now I need RF modulated with square wave.
Thanks