Is mounting the XTAL2 (ref.: page 20, http://focus.ti.com/lit/ds/symlink/cc2480a1.pdf) crystal a waste (of money) when operating in UART mode? The processor can not enter low power state when running in UART mode, as I understand it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I assume you're talking about the external 32kHz for power savings. Since UART mode doesn't support power savings, yes this crystal would be redundant if you were using uart mode.
Ok.
Now, if we assume that we have a system with a RS485 bus, would it then be possible (probably with a few CTS/RTS related tricks) to connect the cc2480 to this bus using a differential bus tranceiver like this one from you: http://focus.ti.com/lit/ds/symlink/sn75176b.pdf ?
Using something like a CTS/RTS based system, would provide the ability to use this edge to wake up the device, provided it is connected to one of the I/Os which has external interrupt capability. This could be used to wake up the device.
One way to "force" the cc2480 to a half-duplex is to raise CTS (trigger on startbit (and other 1s) and stay high for the dureation of a byte) when it gets data on the line and also to let the startbit (and other 1s) of a transmission enable the rs485 driver/disable the receiver (also for the duration of a byte).