This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
jb,
The configurations are contained in the files in this directory.
C:\StellarisWare\SimpliciTI-1.1.1\Components\mrfi\smartrf\CC1101
/Thomas
Thomas,
Ah, I see ... do you think it is valid to use the CC1101 (filename) settings for the TI CC110L which is embedded in the Anaren product? I know they are "close" ...but ...
Assuming that the names in that file have the same meaning as the ones in the Anaren data file, the settings are very different from what they suggest is required to be in line with FCC regulations. What do you think that means? Should I use the ones in the file blindly?
Thanks for your help.
JB
JB,
I would recommend starting with what is inside SimpliciTI today, get your port to work, then contact Anaren FAE's to have them help you figure out which parameters are important and which ones are not.
The two chips are very close to each other, the L version has a few less digital features that I are not commonly used anyway.
Regards
/TA
Whoa Thomas ...Eeek!
You are probably not the right person to address with this, but I seem unable to get off first base with CCS. Attempting to use part of (say) simplicity_cascade into my (internal) CCS5 build ... As soon as I include the linked resource simplicitilib.c and add a simpliciti_config.h I get more compile errors than a dinosaur has feathers. They start with stuff as fundamental as bsp_board_defs.h needing a definition of uint8_t, and go on from there.
I tried to copy all the build includes, but obviously am not "getting it". I'm not even sure what to tell you. Embarrasingly, the simplicity_cascade project compiles just fine. But how do I tell what is the critical difference between my build parameters and its?
Thanks! jb
JB,
I am not the right on, please try posting that question in the Stellaris forum.
/Thomas