I have both CC1101 and CC1070, and I want a very low power, short range (less than 10 m) transceiver system.
1) If I use CC1101, where can I find reference design and layout for 403MHz (I can find only for 433 and 868)?
2) If I use CC1070, which IC can I use as receiver IC that is compatible with it for 402 MHz (also I want refe5rence design for it for 402MHz) ?
If I start with CC1101 for 433MHz, how can I optimize it for 403MHz (any help appreciated) .
Thanks