Hello,
we developed several fantastic applications on the TrxEB+CC1120EMK-169 RF module. At the moment, for a temporary solution I need to have the CC1120EMK-169 connected to a stripboard, where another MSP-based solution resides. Unfortunately, the CC1120EMK-169 has 0.05" connectors from Samtec (SFM-110-02-SM-D-A-K on the RF module and the matching male connectors TFM-110-02-SM-D-A-K on the TrxEB), which are not easily connected to a stripboard, which needs 0.1" throughhole headers. How to connect the RF module to the stripboard?
The only solution it came to my mind was to look on amateur electronic stores for a small PCB adapter to connect the TFM connector to a 0.1" header then soldered on the stripboard.
Any suggestions?