Dear ALL,
The connection of an NFC antenna and NFC transceiver (TRF7970A) is made by TX_OUT/GND, i.e., one terminal of the antenna is connected directly to ground.
For other NFC transceivers such as MLX90132 (Melexis), we have two independent floating (not grounded) connections TX1/TX2 for the same purporse, and I guess this has to be with the tuning for noise reduction.
Which of these two approaches are more powerful regarding impedance matching and noise reduction?
Can we use a two independent connections for the TRF7970A?
At our application is much easier to use two independent connections for the antenna.
Best Regards,
Antonio Stenio (Panasonic Co.)