I have a design using the CC2550 and I am in the process of verifying software from a MSP430. I was attempting to alter the power output, but it doesn't seem to be happening. The CC2550 is being used to generate an unmodulated 2.45 GHz carrier, which is modulated externally and fed into a power amp. It's possible the CCC2550 is in transmit mode at the point where I tried to write to the PATABLE. Can you verify that the PATABLE cannot be written into while in transmit mode? Or perhaps you can write but the new value will not go into effect unless the transmitter is stopped and restarted?
Thanks, Max