Hi
I did few developments involving the CC430F5137 for RF TX/RX @ 915MHz last year and I was very pleased with this component. I was wondering if it would be possible to use this micro-controller as a 162MHz receiver only?
The datasheet indicates the following frequency ranges below but I'm not certain if this is a physical limitation or if it is a legal limitation for TX?
300 MHz to 348 MHz,
389 MHz to 464 MHz,
779 MHz to 928 MHz
I would like to build a tiny AIS receiver (http://en.wikipedia.org/wiki/Automatic_Identification_System).
This is the first time I post a question in the TI forum. Sorry if I did not post this question in the right section.
Regards, Dominique