Hi,
I am using a TRF7970a and a Sony Experia M in peer to peer communication mode. The TRF7970a acts as a passive target. The phone send the SENS_REQ and I get that in TRF7970a. Now TRF7970a replies with SENS_RES but I do not receive any ATTR_REQ from the phone.
I need to find out if the TRF7970a is sending the SENS_RES correctly in passive mode to the phone. Is there a way to make an NFC Sniffer?
Can I use another TRF7970a EVM and configure the TRF7970a of the EVM to act as a silent listener. I know I would be able to get the data sent by the phone since the phone is in active mode, but can I sniff/read what was sent by my passive TRF7970a in reply to the SENS_REQ using the TRF7970a EVM acting as the sniffer.
Regards
Royston