Hi,
I already made some range tests using the two EM included in the DK,
after that I programmet to one of them my application (it did not work as I expected) then I opened the source code for the "per_test_cc2543em".
what happens is that in remote mode I proceed with the configurations selecting by button1, but after selecting the last configuration directly I get "No Beacon Signal" but the other EM is in TX beacon mode!
so what can be the problem?!
also this problematic EM that I reprogrammed, if I choose it as Master I see on the screen "Tx Beacon (10ms)" but when I try in the other EM to be Remote mode is also says "No Beacon Signal".
but when I try the Dongle (Master) whit the EM that I did not programmed, they work good.
Thanks.