All,
I want to use Z-Stack-Lighting to try and build a sample application. I notice that I need to download IAR EW8051, so I did that. I'm a little concerned for hardware, however. I purchased the CC2650EM, which comes with 2 CC2650 Evaluation Modules, and 2 SmartRF06 Evaluation Boards. Upon reading the Sample Application User's Guide for Z-Stack-Lighting, however, I noticed that it mentions only the CC2530 and SmartRF05 boards. Are these the only compliant devices or is there a way I can still build a sample application via the guide with the modules/ boards I have right now?
Thank you!