I purchased the CC2543 development kit that also comes with a CC2544 on a USB dongle, but there is zero information in any of the kit's user guide about how to program this device, other than a single picture of how to hook a cable between the dongle and the RF05 board. What I learned through experimentation is to (1) power-off the RF05 board, (2) attach the dongle to the RF05 through the included cable, (3) attach a USB cable so the dongle has power, and (4) power on the RF05. OK, so far, so good.
Now I start the IAR development environment, compile some code, and attempt to download it through the TI debugger. A window shows me the connected devices, including
"EB ID: 0261 Chip Type:CC0000 EB type: SmartRF05EB"
where the "EB ID: 0261" is the RF05 board. So I select that and then I get "Fatal Error: Failed to identify device" and then the debug session aborts.
Normally, if I'm programming the CC2543 modules also provided with the kit, the "Chip Type" message above will indicate CC2543 and everything works, so clearly it is having a problem with "CC0000".
Has anyone successfully programmed the dongle with this kit? Are there any docs on how to do it?