I just received a SensorTag + Devpack-debug board (the small one that snaps onto the back of the SensorTag). The SensorTag is operational as proven by connecting to iPhone SensorTag app), but what I really want to do is make it transmit Continuous TX such as BT PN9 test pattern. My assumption is that SensorTag + Devpack-debug + SmartRF Studio (or BHET) should be able to achieve this. Is that correct? Assuming so then how to I make that work?
The SensorTag + Devpack-debug has installed OK (Win7 shows Device Manager shows COM3 for UART and COM4 for Aux Data Port). When I open SmartRF Studio7 the device is shown in the 'List of Connected Devices'... but it's identified as "XDS110 (XDS device ID=00000000), -- Unknown". When I open the CC2650 Device Control Panel it opens in offline mode... i.e. not connected to my target device.
What am I doing wrong? Do I need install additonal s/w, or a BTS pack to the device?
Any help/advice/guidence will be much appreciated :)
Regards,
Colin.