Hello all,
I am currently looking at the TRF7970A NFC Transceiver for an NFC Reader/Writer application I am creating. I would like to purchase one of the recommended LaunchPad/BoosterPack Configurations for prototyping purposes. In the Near Field Communication (NFC) reference PDF, I found three possible options including:
1. MSP-EXP430F5529LP + DLP-7970ABP
2. MSP-EXP432P401R + DLP-7970ABP
3. MSP-EXP430F5529 + TRF7970ATB
My question is, while I know these are great options for getting familiar with the functionalities of TRF7970A NFC Transceiver IC without having to worry about developing the RF section and the NFCLink software firmware library, will I be able to write custom code and program the controllers on these devices? I not only need to implement the full ISO/IEC 14443 processes, but also need to create a ISO/IEC 7816-4 challenge-response authentication model. Is this possible on these devices? Also, is there any support for doing something like this?
Thanks!