Hi,
I'd like to use DN0007 to implement IFA into my design.
Took the gerber files from the reference design (CC-Antenna-DK - EtchLayer1Top and CC-Antenna-DK - EtchLayer2).
Looking at the gereber files, it seems that the dimensions are a bit smaller than the ones given in DN0007.
For example L1 from the gerber is 24.66mm, where in DN0007 it is 25.58. The same also for the other dimensions.
Is there really such a difference, or maybe my gerber importer introduced some sort of scaling.
Which one of the sources is more accurate?
Thanks, Isak.