I am developing an NFC Type2/Type4 scanning device using the TRF7970A and the provided firmware (sloc297).
It works very nice, but I'm still looking for any possible improvements on the time a scan takes. Especially when there is no tag present.
I was wondering if the Tx and Rx timeouts are documented somewhere, or if they are defined by trial and error in the firmware. Because the reading process seems to be fine even when I half some of the timeouts.
Thanks in advance!
With kind regards,
Koos