Other Parts Discussed in Thread: CC2640, CC2650
hi,
I want to know which chip support the 5-Mbps (Proprietary) – TX mode, such as CC2640,CC2640R2F,or CC2650
if there is ,can you offer me an example or how can i get an example of this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
we takes pictures continually, and send the pictures through RF to controlling device, by the way analysis the pictures and show them on terminal device. now our RF datarate can reach 3.2Mbps(valid data,not include expenses), we are mow looking for faster RF so we can send larger pictures using the same time.
I head that the cc2640 can reach the datarate of 5Mbps, if not , can you recommend me other chips which can reach a higher TX datarate, and also the example.
thank you!