We are a third party flash programming tool maker.
1. Now we are referring to SLAU603B(RF430FRL15xH Firmware User's Guide) It says that you need to write 0x39 to the JTAG Enable Password Register to enter JTAG mode, but how do we write 0x39 before we enter jtag mode?
2. There's JTAG signature address in SLAS834(RF430FRL15xH NFC ISO 15693 Sensor Transponder) but it doesn’t suggest what the Lock and Unlock values are.
Is it the same as MSP430F where 0x00000000 & 0xFFFFFFFF are Unlock and other values are Lock(SLAU445H doc)?
3. Referring to SLAU320 1.4.3 Testing for a Successfully Protected Device , it means protection is valid when TDI outputs 0xAAAA and then TDO receives 0x5555. And referring to 1.3.2.2.1 Taking the CPU Under JTAG Control, we received a JTAG ID of 0x95(we are not sure if this is correct), and then Bit9 of TDO word won't change to 1 and we have been stuck on this. Is there anything we missed or is this related to my first two questions?
Thanks for your help!
Ryan
overseas@leap.com.tw