Hello~
I use CC2545 basic mode to design my application.
I find a problem and I cannot resolved it over 3 weeks.
The situration as below
1packet is 128byte. TX first byte is 0x7F
RF datarate is 2M, 500K deviation.
In 5ms TX transmit packet twice, the data is same.
Tx first freq. is 2402MHz, second freq. is 2456MHz.
Then Rx is setting as Tx.
The problem is , TX/RX distance over 5Meters, first packet has very high packet error rate(over 5%). Second packet is almost perfect(near 0%).
Please help me to resolve this problem, thanks.
Austin