Hi,
My customer has a question about tuning the LF antenna in RF430F5978.
They were made as shown in the schematic below.
They calculated the value by testing the receive sensitivity by changing the capacitors' capacity of each C16, C18, and C20. (Result - C16 : 86 pF, C18 : 100 pF, C20 : 90 pF)
The test results are as follows:
1) C16 : 86 pF, C18: NC, C20 : NC - Receive distance: 0 ~ 2.5 m
2) C16 : NC, C18: 100 pF, C20 : NC - Receive distance: 0 ~ 2.5 m
3) C16 : 86pF, C18: 100 pF, C20 : NC - Receive distance: 0 ~ 1.2 m
The results of the test show that when a capacitor is connected as shown in 1 and 2, it is received at 2.5 m, but the distance is shorter if connected as shown in 3.
Question :
Is there a problem with the way they test? If there is a problem, please tell me how to test it.
Can the software be used to tune the LF antenna in RF430F5978? If you can, please let me know how.
Best regards,
YJ.