Hello team,
My customer would need presicion after exchange on below exchange on CC2534:
TI feedback :
The CC2534 was a custom part that we offered for select customers so it wasn’t normally accessible from our website. It was a ROMable device that could only be used with pre-configured firmware from TI. It does not support ZRC2.0. However it can be used as a network layer only device in which case the host processor performs the higher layers and in that case could be used to implement ZRC2.0.
However the CC2533F96 does support ZRC2.0 via RemoTI-1.4.0.
Thanks so much for the info re CC2534 and support for ZRC2.0. We are continuing to explore options to support these Charters RF4CE remotes on our XX CC2534 based boxes. Can you provide additional feedback on these follow-up questions?
1. Is the RF4CE MSO profile actually implemented on the CC2534 or is part of it implemented on the Linux side?
2. Does the CC2534 expose the network layer to the Linux side?
3. Does TI already have a version of ZRC2.0 that runs on Linux? If so, is it possible to use that instead of starting from scratch? If not, what level of support would TI be available for?
Thanks in advance for your help,