This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WILINK-BT_WIFI-WIRELESS_TOOLS: Bluetopia platform manager SS1BTPM exit with value 220

Part Number: WILINK-BT_WIFI-WIRELESS_TOOLS

Tool/software: Linux

Hi,

I am using WL1837 module in a IMX6 based custom device. The device has Android Oreo. Bluetooth is up and running and I can able to connect with BT devices.

As part of compliance testing, I am porting SS1BTPM and SS1Tool and try to run on this device. I have run the pre-built binaries present in AM335xBluetopiaLinuxProduction-4.0.3.0.1.0-linux-x64-installer.run and SS1BTPM is immediately exit with error value 220. There is no error messages and so I have no idea what is the reason for the error.

When run the SS1Tool, it exit with the message "Bluetopia Platform Manager service cannot be found. Exiting.".

I have build both these binaries using the toolchain in ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install.bin but this also have the same result, exit with error code 220.

Could you please tell me what is the reason for this problem and how can I proceed with porting SS1BTPM and SS1Tool?

Regards,

Pratheesh