Other Parts Discussed in Thread: RF430F5978
Hi,
I am currently using the RF430f5978 evaluation module and I am testing the MSP access instruction through the MRD2 reader.
The messages sent through the MRD are: 01 11 E8 A0 00 00 32 00 32 40 F3 00 11 22 33 44 99 9A 0A A7
FBCC Start Value: 0x3791
Data: F3 00 11 22 33 44 99 9A
FBCC result: 0x0000
The response I am getting through the MRD is: 01 0C 00 80 7E 00 FF 22 33 44 F1 00 CB 95 F7
FBCC Start Value: 0x3791
Data: 7E 00 FF 22 33 44 F1 00 CB 95
FBCC result: 0x1493
The FBCC calculation value of the MRD2 command is zero, but the FBCC of the LF response is not zero. Is the "Read Frame BCC" in the LF response correctly received?
Is FBCC calculation method of LF response different from MRD2 command?
Thank you,
Jungkil.