Hi everyone,
This question might seem silly but I have to ask. I see that the txPower in dBm is 14 and for that the corresponding value seen in smartrf_settings.c is 0xA73F. The formula for power in dBm is
10*log10[P(in watts)/(1mW)]
When I calculate dBm power from this formula I get
(A73F)16 = (42815)10 = 76.3159 dBm
Or when I try to reverse calculate power value from 14dBm, I get
14 dBm = (0.02511)10= (0.066D9)16
So how do I interpret the values in smartrf_settings? I want to assign a different power value IN THE FILE and cannot do so due to this anomaly.
Can someone help me with this?
Thanks in advance,
-Chandrasekhar DVS