Other Parts Discussed in Thread: CC2650, CC2510, CC2640R2F
Hello,
I am trying to communicate with CC2510 using a CC2650-5X custom board. I am able to establish communication between both on the desired frequency. CC2510 is able to receive on channel number 1 which was set as default in smartRF settings for proprietary mode on transmitter side(CC2650). I don't see any specific field to set the channel number in the Rf receive a command in proprietary mode. How to set the channel to, say 77?
There are two address0 and address1 fields in Rf receive command. Do these signify the channel number anyhow?
Thanks