Other Parts Discussed in Thread: SYSBIOS, CC2650, CC2640R2F
Tool/software: Code Composer Studio
It seems that the examples in the SDK 2.21 (http://dev.ti.com/tirex/explore/node?node=ALYnamhZyxs4QKcXeDSCIw__Drd3Vmn__LATEST
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
It seems that the examples in the SDK 2.21 (http://dev.ti.com/tirex/explore/node?node=ALYnamhZyxs4QKcXeDSCIw__Drd3Vmn__LATEST
For some strange reason, part of the previous post has been cut.
When I build the example rfPacketErrorRate_CC2650DK_7ID_TI I get the following error message:
configuring rfExamples.xem3 from package/cfg/rfExamples_pem3.cfg ...
subdir_rules.mk:19: recipe for target 'build-209907647-inproc' failed
error: xdc.cfg.Program: "C:/ti/ccs1000/xdctools_3_61_00_16_core/packages/xdc/cfg/Program.xs", line 71: xdc.cfg.Program : The package 'ti.sysbios.knl' is not compatible with XDCtools used in this build. Please either use XDCtools compatible with that package, or update the product containing that package, or rebuild the package with XDCtools 3.50 or later.
js: "C:/ti/ccs1000/xdctools_3_61_00_16_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
xdctools_3_61_00_16_core\gmake.exe: *** [package.mak:202: package/cfg/rfExamples_pem3.xdl] Error 1
Can I use multiple versions of XDCtools in CCS 10? (for example 3.31 + 3.61)
Thanks
Regards,
Alberto
I found the examples in http://dev.ti.com/tirex/explore/node?node=ALYnamhZyxs4QKcXeDSCIw__Drd3Vmn__LATEST
I'm trying to build a proprietary protocol using CC2650
The release notes state
https://dev.ti.com/tirex/explore/node?node=AN36.VTBg1KMQkDz9HcTTw__Drd3Vmn__LATEST
You can use later versions of CCS, but then consider selecting the reccomended compiler and xdc toools version.
The CC2640R2F is recommended for new designs, but there is no prop official offering. For more details: