This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RF430CL330H: Look for a transponder for ISO14443

Part Number: RF430CL330H
Other Parts Discussed in Thread: TRF7970A

Hi Team,

 

The customer is looking a transponder which support for ISO14443A, ISO1443B and ISO1443 type-c.

Would you please teach me the device for it?

I think ISO1443 type-c.is ISO18092. Am I correct?

 

I found RF430CL330H supports ISO1443B on ti.com.

Are we still able to emulate ISO 14443A/B transponders using TRF7970A in card emulation mode?

 

Thanks and Best regards,

 Kuerbis

  • Hello Kuerbis,

    ISO14443 Type-C is FeliCa and not ISO18092 though there are similarities.

    We don't have a transponder like the RF430CL330H that emulates ISO14443A/Type A or FeliCa.

    The TRF7970A is able to emulate ISO14443A/Type A and ISO14443B/Type B with provided firmware support.

    The TRF7970A datasheet also states that is capable of emulating FeliCa but we do not have software for that and will not develop such software as the feature is not requested enough (this might be the second time only). The customer would have to implement and validate that on their end.

  • Hi Ralph,

    Thanks!

    Thanks and Best regards,

     Kuerbis