This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8531: Crystal / oscillator for the CC8531

Part Number: CC8531

I have been unable to find a crystal that matches the specifications called for by the data sheet, and the part listed in the demo design is obsolete.

Custom / non stock / long lead time parts are not an option.

The required spec.s per the Data sheet - 48-MHz, ±50 ppm frequency accuracy, load capacitance of 16pF, and max ESR of 60-ohm for proper operation.

The closest I have found are equal or better specifications except this -
One has the load capacitance at 18pF, 60 ohms ESR.
The other is 12pF with 50 ohms ESR

Is there a way to reliably adapt anything to use these, or do I have to resort to an oscillator?  They are available, but cost much more than a crystal.

Thank you,

Dave