This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC-DEBUGGER: CC-debugger is not recognized (application for CC85XXDK-Headset)

Prodigy 70 points

Replies: 4

Views: 260

Part Number: CC-DEBUGGER

Hi ,

Noted  CC-Debugger-User's Guide Page 16-19

 

8.2 Updating the firmware manually in SmartRF Flash Programmer
 loading sucessful ,but cc-debuger not  recognized

8.4 Resurrecting the CC Debugger

operated software" Texas Instruments SmartRF Flash Programer"

download "EB application"  ------->cebal_fw_srf05dbg.hex   it is OK

but in EB booloader ,the table of EB ID can't find out device (it is null) so it can't loading files

 

need we change IC CC2511?

 

Thanks

 

Charlin
 

  • Guru 227235 points
    If the method described under "8.4 Resurrecting the CC Debugger" does not work it sounds like the debugger has been damaged and you should get a new one.

     Out of office, back 20.06

  • In reply to TER:

    Thank your reply!

    The CC-Debuger is brought from www.mouser.com ,if don't have clear evidence, they can't rechange the new one

    if we can try to resurrect it  well ,need not to  argue with supplier

    Do you think what happened to device ,CC2511 has been damaged?

    Thanks

    Charlin 

  • Guru 227235 points

    In reply to Charlin user1151140:

    As in get I meant buy a new one. See e2e.ti.com/.../763015 on where you can get a new one.

    The debugger could potentially have been damaged by ESD.

     Out of office, back 20.06

  • I had a similar problem running Win 10 on a 64-bit computer.  The CC Debugger was showing up in device manager, but the entry showed that there was no driver installed, event though the normal installation procedure was used for installing the SmartRF Flash Programmer.  I found the required driver, cebal2_x64.exe, in http://www.ti.com/lit/zip/swrc212

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.